Technical FAQs

Ask a Question

Will a HOM612L100S load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 6 space/12 circuit panel, accepting a maximum of (6) HOMT tandem or (3) HOMT quad tandem circuit breakers.


CTA-ID : 2002235
Was this helpful?
What can we do to improve the information ?