Technical FAQs

Ask a Question

Will a HOM24L70F load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 2 space/4 circuit panel, accepting a maximum of (2) HOMT tandems or (1) HOMT quad tandem circuit breaker.

CTA-ID : 2002231
Was this helpful?
What can we do to improve the information ?