Technical FAQs

Ask a Question

What is the wire range of the Main Lugs of a QON42LS400 load center?

The Main Lugs will accept (1) 1/0 AWG - 750 kcmil or (2) 1/0 AWG - 300 kcmil aluminum or copper conductors per phase.

CTA-ID : 2002017
Was this helpful?
What can we do to improve the information ?