Technical FAQs

Ask a Question

Can the Generator Kit, part number QCGK3 be used with the QO load centers?

Issue:
Product design feature

Product Line:
QO load centers

Environment:
Generator kit accessory

Cause:
Application

Resolution:
The QCGK3 is NOT designed for use in QO load centers. It is designed for use ONLY with the QC816F...* and QC2442M...* Combination Service Entrance Devices.


CTA-ID : 2002014
Was this helpful?
What can we do to improve the information ?