Technical FAQs

Ask a Question

What are the deadfront part numbers for an NQOD42L600TFL or NQOD442L600TFL interior?

Each panel will require the following:

SINGLE PHASE INTERIOR
(1) 80116-325-56
(1) NQODRPL42L6TFL

THREE PHASE INTERIOR
(1) 80116-325-56
(1) NQODRPL442L6TFL


CTA-ID : 2002010
Was this helpful?
What can we do to improve the information ?