Technical FAQs

Ask a Question

What are the dimensions of the QOC24US load center cover?

Issue:
Dimensions

Product Line:
QO Load Center

Environment:
Dimensions

Cause:
Dimensions

Resolution:
This cover is 20.92`` H x 14.24`` W. The surface cover will be the same height and width as the load center it is mounted to.


CTA-ID : 2001746
Was this helpful?
What can we do to improve the information ?