Technical FAQs

Ask a Question

What are the dimensions of a QOC12UF load center cover?

Issue:
Dimensions

Product Line:
QO Load Center

Environment:
Dimensions

Cause:
Dimensions

Resolution:
This cover is 16.12" H x 15.44" W. The cover will overlap the load center enclosure by .60`` (19/32``) on all sides.


CTA-ID : 2001735
Was this helpful?
What can we do to improve the information ?