Technical FAQs

Ask a Question

What are the overall dimensions of the QOC16UF load center cover?

Issue:
Product features

Product Line:
QO Load centers

Environment:
Cover dimensions

Cause:
installation

Resolution:

This cover is approximately 19.12" H x 15.44" W. The cover will overlap the load center enclosure by approximately 0.60" (19/32``) on all sides for flush mount applications.


CTA-ID : 2001736
Was this helpful?
What can we do to improve the information ?