Technical FAQs

Ask a Question

How does one order contact blocks factory installed on a 9001 30mm operator?

After determining the type of contact block required and the desired mounting positions, select the apropriate H code. The mounting position is in relation to the locating notch on the top of the operator.





CTA-ID : 2002477
Was this helpful?
What can we do to improve the information ?