Technical FAQs

Ask a Question

Is there any type of extension kit available for QMB interiors so they can be mounted in a larger enclosure?

No. Extensions kits are not offered for QMB interiors due to the weight and configuration of the interior.


Revised 3/10/04



CTA-ID : 2002463
Was this helpful?
What can we do to improve the information ?