Technical FAQs

Ask a Question

Are the 7LM type CTs still available? Are there published specifications?

The 7LM series current transformers are still available as of February of 2003. It is a military rated product siold only to OEMs making equipment for the military through a few authorized distributors. There is no publicly available standard published catalog data.


CTA-ID : 2002459
Was this helpful?
What can we do to improve the information ?