Technical FAQs

Ask a Question

What are the NEMA ratings of the 9001 30 mm control station enclosures?

The 9001 KYAF and KZ `s are rated NEMA 1, 3. and 13.
The 9001 KY `s are rated NEMA 1, 3, 4, and 13.
The 9001 KYSS and SKY `s are rated NEMA 1, 3, 4, 4 X, and 13.

See View.


CTA-ID : 2002450
Was this helpful?
What can we do to improve the information ?