Technical FAQs

Ask a Question

Will a HOM42L225C load center accept a HOMT tandem or quad tandem circuit breaker?

Issue:
Application

Product Line:
HOM LC

Cause:
Clarification if HOMT tandem breakers can be used

Resolution:
No, it will not. This is a 42 space/42 circuit panel, accepting full size HOM branch breakers only.


CTA-ID : 2002193
Was this helpful?
What can we do to improve the information ?