Technical FAQs

Ask a Question

Can I get ring tongue terminal connections for accessory wiring instead of the standard push-in connector on the Masterpact NT circuit breaker?

No. The NT was designed to be a very small breaker. The ring tongue terminals are too large. The push-in connectors help maintain the small NT footprint. If ring tongue terminals are required, then use the larger NW breaker.


CTA-ID : 2001990
Was this helpful?
What can we do to improve the information ?