Technical FAQs

Ask a Question

Are replacement parts available for the old style, i.e. pre-Series D (IGD), Line Isolation Monitors (LIM)?

No replacement parts are available for these devices.  The IGD is a direct replacement for all previous Square D Line Isolation Monitors.  The replacement IGD is shipped with all the components necessary to replace an earlier series Square D line isolation monitor.  The IGD also replaces other manufacturer`s LIMs, though a mounting adapter kit may be required.  If necessary, concact Square D Medical Products for guidance.

CTA-ID : 2001982
Was this helpful?
What can we do to improve the information ?