Technical FAQs

Ask a Question

Is the face plate (back plate behind the reset button area) replaceable on the XY2CE devices?

No the faceplate is not replaceable.
All replaceable parts are listed in; D172, pgs. 17-31, 17-32.


CTA-ID : 2002189
Was this helpful?
What can we do to improve the information ?