Technical FAQs

Ask a Question

Is the HCWM-U interior still available?

No. The HCWM-U has been replaced by the HCR-U. The enclosure for the HCR-U is 86H x 44W x 9.5D (HC4486DB). The HCR-U has mounting provisions on the ``narrow`` side of the bus stack for 250A max. ``K`` frame breakers.


CTA-ID : 2002186
Was this helpful?
What can we do to improve the information ?