Technical FAQs

Ask a Question

Can the ATV66 Drive run without a keypad installed?

The Altivar 66 can operate with the keypad display removed if it is not in keypad command.


CTA-ID : 2002180
Was this helpful?
What can we do to improve the information ?