Technical FAQs

Ask a Question

Is the cover of a QO816L100RB load center side hinged or top hinged?

Issue:
Product Design features

Product Line:
QO load centers

Environment:
Cover

Cause
Installation

Resolution:

The cover on this load centers is top hinged.


CTA-ID : 2001697
Was this helpful?
What can we do to improve the information ?