Technical FAQs

Ask a Question

Is the cover of a QO24L60NRNM load center side hinged or top hinged?

Issue:
Product design features

Product line:
QO load centers

Environment:
Cover operation

Cause:
Application

Resolution:
This device is side hinged.


CTA-ID : 2001691
Was this helpful?
What can we do to improve the information ?