Technical FAQs

Ask a Question

Can a QON42LS400 load center be either top or bottom fed?

This load center interior can be mounted into the enclosure with the Main Lugs positioned at the top (for top feed applications) or at the bottom (for bottom feed applications) of the enclosure. No field modifications are required.
NOTE: When the interior is rotated, the deadfront trim labels will be upside down. The labels should, if handled carefully, be able to be removed and repositioned for proper orientation.


CTA-ID : 2002401
Was this helpful?
What can we do to improve the information ?