Technical FAQs

Ask a Question

When does the XSAV`s output open and close?

As long as the target speed stays above the set threshold level the output circuit will assumes its closed state. When the actual speed drops below the set threshold level the output circuit changes to its open state.


CTA-ID : 2002164
Was this helpful?
What can we do to improve the information ?