Technical FAQs

Ask a Question

Is it possible to get (1) 240Vac, 30 ampere circuit and (2) 120Vac, 20 ampere circuits using load center QO24L70RB?

No. However, this application can be satisfied in the HOMELINE product line. Consider HOMT2020230 circuit breaker and HOM24L70RB load center.


CTA-ID : 2001930
Was this helpful?
What can we do to improve the information ?