Technical FAQs

Ask a Question

Can 9998LH style replacement coils be used for the 2 to 6 pole 8903 Type L, and 2 to 4 pole 8903 Type LX lighting contactors?

The 9998LH coils are physically the same size as the 9998L coil; however, their use as replacements for the 9998L has the potential to degrade the operation of the contactor over time and is not recommended.


CTA-ID : 2002383
Was this helpful?
What can we do to improve the information ?