Technical FAQs

Ask a Question

How do I assign Reference Switching to a Logic input in the ATV28?

Issue:   How do I assign Reference Switching to a Logic input in the ATV28?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   
From factory I/O settings it will be necessary to set the LI4 then LI3 inputs to some setting that is compatible with Reference Switching. Preset speeds are incompatible with Reference Switching. LI4 must be changed before LI3. If not using LI3 or LI4 set them to NO.

In the I-O menu change the desired logic input to rFC. It will be in Auto and use AI2 or AIC for speed reference when the contact is open. The drive will be in Hand mode and use AI1 for speed signal when there is 24 VDC on the rFC input.


 
Was this helpful?
What can we do to improve the information ?