Technical FAQs

Ask a Question

What Neutral Assembly is used with a MA1000F, MA1000R or MA1000S circuit breaker enclosure?

Use a AL800SN when using a 300-1000 ampere MAL or MHL circuit breaker. Use a 400SN when using a 125-400 ampere Q4L, LAL or LHL circuit breaker. Use a SN1000MA when using a 450-800 ampere MXL circuit breaker with integral ground fault protection.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2001929
Was this helpful?
What can we do to improve the information ?