Technical FAQs

Ask a Question

Why does the drive not run when closing a contact from LI1 to +24?

It is also necessary to provide a speed signal. This can be done using the analog inputs or logic inputs for preset speeds. The drive will run at Low Speed (LSP) if there is no speed signal provided. The default low speed is 0. Therefore, you could use the LSP to control the speed as well.


CTA-ID : 2002139
Was this helpful?
What can we do to improve the information ?