Technical FAQs

Ask a Question

From what material is a B-Hub made?

Issue:
Product Characteristics

Product Line:
Accessories

Environment:
B-hubs

Cause: 
Need to know material of B-hubs

Resolution:
B-hubs, 3/4`` through 2 1/2`` are zinc.
B-hubs, 3`` through 4`` are aluminum.

The blank cover, bcap, that comes standard on all RB devices is grey painted plastic.
Was this helpful?
What can we do to improve the information ?