Technical FAQs

Ask a Question

Why do we have to use a copper interior on the 400A NQOD panels when it goes into a NEMA 3R,5,12 enclosure?

We use copper interiors on 400A NEMA 3R,5,12 panels due to the heat rise on the 400A panels in non-vented enclosures.

CTA-ID : 2001634
Was this helpful?
What can we do to improve the information ?