Technical FAQs

Ask a Question

What Filler Plate is used to fill the main circuit breaker opening in HOMELINE convertible main breaker load center covers?

Issue:
Selection

Product Line:
Homeline load centers

Environment:
Filler plates

Cause:
Selection

Resolution:
Use QOM1FP for 100 - 125 ampere, Series S1, S2, S3 or S4, convertible main breaker devices. Use QOM2FP for 150 - 225 ampere, Series S1, S2, S3 or S4 convertible main breaker devices.


CTA-ID : 2001631
Was this helpful?
What can we do to improve the information ?