Technical FAQs

Ask a Question

Will the GC200 system work on a single phase system?

Yes. The GC200 relay will provide GFP on single phase circuits. The hot and neutral need to go through the sensor.


CTA-ID : 2002125
Was this helpful?
What can we do to improve the information ?