Technical FAQs

Ask a Question

What is the Equipment Gound Kit for a HU661AWK safety switch?

An Equipment Ground Kit is provided factory installed in this device (Series F design). Two lugs are provided, each capable of terminating (1) #14 - 1/0 AWG copper or (1) #12 - 1/0 AWG aluminum.

CTA-ID : 2001875
Was this helpful?
What can we do to improve the information ?