Technical FAQs

Ask a Question

Is a field installable neutral assembly available for a QON2L70 OEM interior?

The QON2L70 is for 1-Phase, 2-Wire, 240Vac systems. No neutral can be field installed. Consider using a QON2-4L70, which has a neutral and would be suitable for 1-Phase, 3-Wire, 120/240Vac systems.


CTA-ID : 2001870
Was this helpful?
What can we do to improve the information ?