Technical FAQs

Ask a Question

Can a single pole FAL breaker be applied in a FA100DS circuit breaker enclosure?

This enclosure is UL Listed and marked for use with a 1-pole, 2-pole or 3-pole FAL, FHL or FCL circuit breaker. This information is valid as of January 30, 2003. Devices manufactured before this date will not have the 1-pole schematic on the wiring diagram, although the 1-pole breaker will physically mount into the enclosure. This information is also valid for FA100A, FA100AWK, FA100F, FA100RB and FA100S.

CTA-ID : 2002105
Was this helpful?
What can we do to improve the information ?