Technical FAQs

Ask a Question

What is the cycle time for a PAMO2 operator for the PA?

OFF to ON is approx. 0.4 seconds, ON to OFF is approx. 0.4 seconds. Control signal duration should be at least 0.1 sec. For OFF-ON-OFF, it would take one second conservatively.


CTA-ID : 2001866
Was this helpful?
What can we do to improve the information ?