Technical FAQs

Ask a Question

Can an Arc Fault breaker be used on a ceiling light load ?

Yes and it could also handle some other loads too as long as one neutral was used throughout the circuit


CTA-ID : 2001853
Was this helpful?
What can we do to improve the information ?