Technical FAQs

Ask a Question

Customer needs installation assistance with GAT12. Trying to test this ground fault relay with a 5000 to 5 CT.

GA sensor is required for use and testing of the GA relay. These sensors are not common ratio CT`s. These sensors output a voltage signal, rather than a linear current, proportionate to the non zero sequenced current through the window.


CTA-ID : 2002099
Was this helpful?
What can we do to improve the information ?