Technical FAQs

Ask a Question

Are there any maintenance recommendations concerning the cleaning of a HOMELINE load center interior?

Issue:
Maintenance

Product Line:
Homeline LC

Cause:
Maintenance Recommendation

Resolution:
For general cleaning, disconnect all power feeding the load center and remove the branch circuit breakers from the panel interior. Use a vacuum to remove any lose dirt from the interior. Wipe down the interior with a dry, lint free cloth. Do not use any petroleum based products. Allowing petroleum base paint, solvents or spray to contact the non-metallic parts of this product may adversely affect user safety and impair reliability.
NOTE: If the load center has been submerged it should be replaced. 


CTA-ID : 2002042
Was this helpful?
What can we do to improve the information ?