Technical FAQs

Ask a Question

When using EDB, EGB or EJB breakers rated 110A or less, is there a limitation on what breaker can be mounted across from them?

The sum of the two breaker combination must be restricted to no more than 170A. ( Example: 170A - EDB34110 = 60A MAX across from the 110A breaker.)

CTA-ID : 2001844
Was this helpful?
What can we do to improve the information ?