Technical FAQs

Ask a Question

What is the Terminal Lug Data for a D226NR, Series E1 General Duty safety switch?

Issue:
Product Design Features

Product Line:
General Duty Safety Switches

Environment:
Lug data

Cause:
Installation

Resolution:

The lugs on this device will accept (2) #4 AWG - 600 kcmil copper or aluminum conductors per phase. However, wire bending space available in the switch restricts the conductors to (2) 500 kcmil maximum.


CTA-ID : 2001588
Was this helpful?
What can we do to improve the information ?