Technical FAQs

Ask a Question

What is the Terminal Lug Data for a D326NR, Series E1 General Duty safety switch?

The lugs on this device will accept (2) #4 AWG - 600 kcmil copper or aluminum conductors per phase. However, wire bending space available in the switch restricts the conductors to (2) 500 kcmil maximum.

CTA-ID : 2001590
Was this helpful?
What can we do to improve the information ?