Technical FAQs

Ask a Question

What is the Terminal Lug Data for a D325NR, Series E1 General Duty safety switch?

Issue:
Lug data

Product Line:
GD SS

Cause:
Clarification of terminal lug data

Resolution:
The lugs on this device will accept (1) #1/0 AWG - 600 kcmil or (2) #1/0 AWG - 250 kcmil copper or aluminum conductors per phase. However, wire bending space available in the switch restricts the conductors to (2) 250 kcmil maximum.


CTA-ID : 2001579
Was this helpful?
What can we do to improve the information ?