Technical FAQs

Ask a Question

What Class R Fuse Kit is used with the D224N, D224NRB, D324N and D324NRB General Duty safety switch?

Issue:
Selection

Product Line:
GD SS

Cause:
Selection of Class R Fuse Kit

Resolution:
The correct Class R Fuse Kit is dependent upon the Series number of the safety switch. For Series D2 or E1 - E4, use DRK1020. For Series F01, use HRK1020.


CTA-ID : 2002324
Was this helpful?
What can we do to improve the information ?