Technical FAQs

Ask a Question

Is it possible to get (1) 240Vac, 20 ampere circuit and (2) 120Vac, 20 ampere circuits using load center QO24L70RB?

Yes, by purchasing (2) QOT2020 circuit breakers and a QOTHT handle tie which will allow common switching (not commom trip) of the two center poles for the 240Vac circuit and the two outer poles used for 120Vac circuits.

CTA-ID : 2001830
Was this helpful?
What can we do to improve the information ?