Technical FAQs

Ask a Question

What is the Terminal Lug Data for a D325NT, Series E3 General Duty safety switch?

The lugs on this device will accept (1) #1/0 AWG - 750 kcmil or (2) #1/0 AWG - 300 kcmil copper or aluminum conductors per phase. However, wire bending space available in the switch restricts the conductors to (1) 600 kcmil or (2) 300 kcmil maximum.


CTA-ID : 2001576
Was this helpful?
What can we do to improve the information ?