Technical FAQs

Ask a Question

Can a Nano Connector be used on a Micro Connector Sensor

NO, A Nano style connector has a M8 X1 thread and the Micro style connector has a M12 X1 thread. Two different sizes which can not be interchanged.


CTA-ID : 2000417
Was this helpful?
What can we do to improve the information ?