Technical FAQs

Ask a Question

Are optional lugs available for the SN400LA neutral assembly?

Issue:
Product Features

Product Line:
CB Enclosure Accessory

Cause:
Optional Lugs

Resolution:
Yes, optional lugs are available for the SN400LA neutral assembly. The standard lug provided on the neutral assembly will accept (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil CU or AL conductors. Optional lugs include: AL400LH7 for (1) 350 -750 kmcil CU or AL conductor: CU400LA for (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil CU only conductors. The optional lug kits contain one lug. Two kits would be required to change both the incoming and outgoing neutral lugs.


CTA-ID : 2001794
Was this helpful?
What can we do to improve the information ?