Technical FAQs

Ask a Question

Are optional lugs available for the SN1200NACT neutral assembly?

Yes, optional lugs are available for the SN1200NACT neutral assembly. The standard lugs provided on the neutral assembly will accept (4) #3/0 AWG - 600 kcmil CU or AL conductors. Optional lugs include: CU1200NE6 for (4) #3/0 AWG - 600 kcmil CU only conductors. The optional lug kit contains one lug. Two kits would be required to change both the incoming and outgoing neutral lugs.

CTA-ID : 2001790
Was this helpful?
What can we do to improve the information ?