Technical FAQs

Ask a Question

What is the load base assembly for the PQ4606G and the PQ3606G plug-in units?

Part number is 45201-624-50. One of these parts replaces all 3 phases. This applies to Ser 4 plug-in units only.

CTA-ID : 2002044
Was this helpful?
What can we do to improve the information ?