Technical FAQs

Ask a Question

Can side gutters be added to both sides of an HC26XXB NEMA 1 box? If so, what is the maximum width that each gutter can be?

Side gutters with a maximum width of 3`` can be added to each side of an HC26XXB NEMA 1 box.

CTA-ID : 2002494
Was this helpful?
What can we do to improve the information ?